Technical FAQs

Ask a Question

Error Message after ION Enterprise Installation

Summary

After installing ION Enterprise, the following error message might be generated when one tries to open the Management Console

"Cannot create the helper component required to start the application."

Resolution

The install has not completed. You need to reboot the machine to complete the install.

 

Original article#9846, SWKB-0457


Legacy KB System (APS) Data: RESL182721 V1.0, Originally authored by DaMi on 03/14/2007, Last Edited by DaMi on 03/14/2007
Related ranges: ION Enterprise
Was this helpful?
What can we do to improve the information ?