Technical FAQs

Ask a Question

ION Enterprise Designer Handling Of Shortcut Paste Operation

Goals and Symptoms

If a framework file contains a shortcut but not the module that the shortcut references, a new module will be created if the shortcut exists in the source framework.

This behavior does not occur for core modules, as core modules cannot be created.

Causes and Fixes

If this behavior is undesirable, use one of the following methods to avoid it
* Don't include shortcuts when selecting modules to be copied.
* Ensure that the module that the shortcut references is also copied.

Original article#9629, SWKB-0042


Legacy KB System (APS) Data: RESL182691 V1.0, Originally authored by DaMi on 03/14/2007, Last Edited by DaMi on 03/14/2007
Related ranges: ION Enterprise
Was this helpful?
What can we do to improve the information ?