Technical FAQs

Ask a Question

ION Enterprise Vista Response To Object Move Operation Is Delayed - Vista Undo Option

Goals and Symptoms

A significant lag time can be observed between dragging a diagram object and resulting movement on Vista diagrams that consist of many objects. Diagrams that consist of few objects do not exhibit this behaviour.


Causes and Fixes

Resolution

To speed the process of editing Vista diagrams, the user can disable Undo operations by unchecking the Enable Undo item on the Options menu.

 



Background

Vista offers the ability to enable or disable undo operations in Vista through the Options menu item called Enable Undo. If Enable Undo has is checked, undo operations are enabled and the user can revert any individual changes made to the diagram. Undo operations are disabled by default; however, a user's last setting is saved into and restored from their Vista workspace file. Disabling undo operations while editing busy Vista diagrams serves to speed up the process significantly because no extra processing needs to be done before a change is reflected in the diagram.

 

Original article#9625, SWKB-0013


Legacy KB System (APS) Data: RESL182684 V1.0, Originally authored by DaMi on 03/14/2007, Last Edited by DaMi on 03/14/2007
Related ranges: ION Enterprise
Was this helpful?
What can we do to improve the information ?