Technical FAQs

Ask a Question

How To Import Data Into Access From ION Database

Goals and Symptoms

How To Import Data Into Access From ION Database

Causes and Fixes

To set up an ODBC data source:
* From the control panel, start the ODBC (Data Sources) applet.
* Click on the System DSN tab.
* Press the Add button.
* On the Create New Data Source dialog, double-click on the Sybase SQL Anywhere 5.0 driver.
* In the Data Source Name field on the SQL Anywhere ODBC Configuration dialog, enter a name for the data source
* Press the Browse button and locate the database from which data will be imported.
* Press the OK button to accept the Data Source configuration.

To import data into Microsoft Access:
* Start Microsoft Access
* From the File menu, select GetExternalData    - Import
* On the Import dialog, select ODBC Databases as the file type.
* On the Select Data Source dialog, click the Machine Data Source tab and select the Data Source Name associated with the source database.
* Enter the following user ID: DBA
* Enter the following password: SQL
* On the Import Object dialog, select the tables to be imported and click OK.

The data should appear in the Access database.

Original article#9581, SWKB-0059


Legacy KB System (APS) Data: RESL182677 V1.0, Originally authored by DaMi on 03/14/2007, Last Edited by DaMi on 03/14/2007
Related ranges: ION Enterprise
Was this helpful?
What can we do to improve the information ?