Technical FAQs

Ask a Question

Adding ION Devices to ION Enterprise through an EGX Gateway

See attached ION Knowledge Base article.
Adding devices through EGX Gateway.pdf


Please Read:

The above article details the procedure for adding ION devices to an ION Enterprise system through an EGX100 gateway. This process is necessary due to protocol conflicts. The EXG100 speaks Modbus protocol, where ION Enterprise expects ION meters to speak ION protocol when connecting to them. The exception to this is the ION 6200, which has a native Modbus driver to allow it to speak Modbus protocol to ION Enterprise.


Legacy KB System (APS) Data: RESL182364 V2.0, Originally authored by DaMi on 02/27/2007, Last Edited by MaTh on 10/12/2012
Related ranges: ION Enterprise V5.5
Was this helpful?
What can we do to improve the information ?