Technical FAQs

Ask a Question

Site Auto-Disconnect Feature with Custom Log Inserter

Goals and Symptoms

Summary

The Auto-Disconnect feature does not work with a custom Log Inserter when the Log Acquisition module is disabled.

 

Facts and Changes

 Keywords

Connection schedule, Auto-disconnect, Custom Log Inserter, Log Acquisition module

 

Causes and Fixes

Symptoms

When the Log Acquisition module is disabled and a connection is made to a site, that site does not disconnect after all logs have been retrieved even when the Disconnect from each site as soon as all data has been retrieved option is selected.

 Cause

All logs requiring retrieval must be up to date for the Auto-Disconnect feature to work.

From the Log Acquisition module description in the ION Reference:

When [the Enable] input is set to on, the module is enabled; when it is set to off, the module is disabled and logs are not uploaded.

The Log Acquisition module is not considered caught up when the logs are not updated.

 

Original article#10766

All content © 1992-2005 Power Measurement


Legacy KB System (APS) Data: RESL182117 V1.0, Originally authored by DaMi on 02/13/2007, Last Edited by DaMi on 02/13/2007
Related ranges: ION Enterprise
Was this helpful?
What can we do to improve the information ?