Technical FAQs

Ask a Question

What is the maximum number of concurrent Ethernet connections that the Powerlogic EGX400 supports?

The Powerlogic EGX400 is a Modbus to Ethernet gateway that can support a maximum of 10 concurrent Ethernet (Modbus TCPIP) connections.


Legacy KB System (APS) Data: RESL180619 V1.0, Originally authored by DaSo on 11/29/2006, Last Edited by DaSo on 11/29/2006
Related ranges: EGX400
Was this helpful?
What can we do to improve the information ?