Technical FAQs

Ask a Question

How to Transfer System Manager Software Professional Edition Version 4.0.3 (SMSPE v4.0.3) and SMSOPC to a New Server

Issue:
Obtain information on what files and databases need to be backed up, moved and restored to Transfer SMSPE V4.0.3 and SMSOPC to a New Server.

Product Line:
System Manager Software Profession Edition Version 4.0.3 (SMSPE v4.0.3)
SMS OPC Server (SMSOPC)

Cause: 
Moving SMS to another machine, device, transferring, migrate, migrating SMS.

Resolution:
See attached document for the information.


Legacy KB System (APS) Data: RESL198386 V1.0, Originally authored by AnVa on 04/29/2009, Last Edited by AnVa on 04/29/2009
Related ranges: SMS Add-on, System Manager 4.0
Was this helpful?
What can we do to improve the information ?