Technical FAQs

Ask a Question

Masterpact NT and NW, PowerPact P and R-Frame, and Compact NS Modbus Communication User Guide/Register List

Issue
Masterpact (NT and NW) and larger frame size Powerpact (P and R Frame) and Compact NS Circuit Breakers use different communication parameter and device then other Micrologic circuit like the PowerPact H- J- and L-Frame and Compact NSX Circuit Breakers. See FA226079 for information on the other breakers.
 
Product Line

Trip Unit Trip Function Type
2.0 (IEC Only) LSO Standard (No comms)
3.0 LI
5.0 LSI
2.0A (IEC Only) LSO Standard
3.0A LI
5.0A LSI
6.0A LSIG
5.0P LSI Power
6.0P LSIG
5.0H LSI Harmonics
6.0H LSIG

 
Environment
Communication applications using Micrologic trip units and circuit breakers with frame sizes 630 A and greater.

Cause
Need register lists and a communication guide for Micrologic trip unit.

Resolution
The below are the links to the Modbus user guides.
 
Masterpact NT/NW and PowerPact™ P- and R-Frame Modbus Communication Guide 0613IB1313
 
Masterpact NT/NW, Compact NS Modbus Communication Guide DOCA0054EN

Attached is the legacy user guides

Was this helpful?
What can we do to improve the information ?