Technical FAQs

Ask a Question

How do I correct overlapping text on Multi-Device Electrical Usage Pie Chart when using Advanced Reports.

Issue:
Overlapping text on Multi-Device Electrical Usage Pie Chart when using Advanced Reports.

Product Line:
System Manager Software (SMS) 4.x

Environment:
System Manager Software Advanced Reports
 
Causes:
The PowerLogic.Reports.History.MultiDevElectricalUsage.rpt file need to be refreshed.

Resolution:
Please do the following to install the new report.
1. Transfer the PowerLogic.Reports.History.MultiDevElectricalUsage_new.rpt located in this directory to the customer.
2. Browse to \Powerlogic\Advanced Reports\Webcontent\Reports
3. Rename PowerLogic.Reports.History.MultiDevElectricalUsage.rpt to PowerLogic.Reports.History.MultiDevElectricalUsage_old.rpt
4. Transfer the attached file and save it to \Powerlogic\Advanced Reports\Webcontent\Reports
5. Rename PowerLogic.Reports.History.MultiDevElectricalUsage_new.rpt to PowerLogic.Reports.History.MultiDevElectricalUsage.rpt
6. You must create a new report to see the change. Existing reports will not be automatically updated.
Was this helpful?
What can we do to improve the information ?