Technical FAQs

Ask a Question

Can we change default logging interval of Powerlogic meters(CM4000, CM3000, PM800, and/or PM600) in ION E 6.0/SPM 7.0.1?

Issue
User wants to change the logging interval for Powerlogic meters(CM4000, CM3000, PM800, and/or PM600)

Product Line
CM4000, CM3000, PM800, and/or PM600
ION setup
ION 6.0
Structureware Power Monitoring 7.01
Power Management Expert 7.2.

Environment
Meter configuration using ION6.0, SPM, or PME

Cause
ION 6.0,Structureware Power Monitoring 7.01, and Power Management Expert 7.2. does not have the capability to change the logging interval for the onboard log files

Resolution
The onboard logging interval can be changed using ION setup. However, StruxureWare Power Monitoring 7.0, and Power Management Expert 7.2 will not extract Data logs from the meter with an interval at or less than 1 minute. A Work around would be to create data recorders in the VIP which can log data from the Powerlogic meters at intervals of 1 minute or less. Consider the size and complexity of the VIP and system before such configuration.


Legacy KB System (APS) Data: RESL212648 V2.0, Originally authored by ChMu on 10/02/2013, Last Edited by DaWa on 12/14/2013
Related ranges: Power Monitoring Expert 7
Was this helpful?
What can we do to improve the information ?