Technical FAQs

Ask a Question

Does the Power Monitoring Expert/StruxureWare Power Monitoring Web Applications support Active Directory integration?

Issue: 
When accessing the web applications of PME/SPM, the user must log in each time. 

Product Line:
Power Monitoring Expert 8.0
Power Monitoring Expert 7.2.x
Struxtureware Power Monitoring 7.0.x

Environment:
Web Applications

Cause: 
When accessing the web portion of SPM7/PME, the user must log in each time. With Active Directory Integration and/or LDAP, the user would not need to log in each time.

Resolution:
This capability is not currently supported/implemented within SPM/PME or any previous versions of our software.

Was this helpful?
What can we do to improve the information ?