Technical FAQs

Ask a Question

Are the CM4000 circuit boards coated with a fungus resistant material or is the option available for order?

Issue
Fungus resistant circuit boards

Product Line
CM4000

Environment
Hardware 

Cause
Fungus resistant circuit boards

Resolution
The CM4000 circuit boards are not coated with anti-fungus material, nor is the option available. The closest available replacement is the tropicalization treatment on the ION7650. This is option C under special order options.

Was this helpful?
What can we do to improve the information ?