Technical FAQs

Ask a Question

What registers hold the DL, OS, LL, and CVMT firmware versions of the CM4000?

Issue
Which registers hold DL, OS, LL, and CVMT firmware versions of the CM4000?

Product Line
CM4000

Environment
Register Mapping

Resolution

Register Mapping
Item Register
OS 3014
LL 3015
DL 3016
CVMT Firmware 3017
Was this helpful?
What can we do to improve the information ?