Technical FAQs

Ask a Question

What are the screw size and wire sizes for the CT and PT terminal connections on the CM3000 series meters?

Issue:
A user requires the information of the screw size and wire sizes, for the CT and PT terminal connections on the CM3000 series meters.

Product Line:
CM3000 series meters

Cause:
A user requires the information of the screw size and wire sizes, for the CT and PT terminal connections on the CM3000 series meters.

Resolution:
The terminal screws are 6-32 standard screws. Each meter is supplied with spade lugs that accommodate 14-16 AWG wire.

Was this helpful?
What can we do to improve the information ?