Technical FAQs

Ask a Question

Remote Display Cable information for CM4000, CM3000 and PM800 series meters.

Issue
What are the part numbers for the remote display cables used in the CM4000, CM3000 and PM800 series meters? 

Product Line
CM3000
CM4000
PM800

Environment
Product Specifications

Cause
What are the part numbers for the remote display cables used in the CM4000, CM3000 and PM800 series meters? 

Resolution
The part numbers for the cables are CAB4, CAB12, and CAB30 and correspond to lengths of 4, 12 and 30 feet. 
 
Was this helpful?
What can we do to improve the information ?