Technical FAQs

Ask a Question

What is the Panel Mount RJ11 Extender Connector Kit for the CM3000/CM4000/PM800 Series of monitors?

Issue
Panel Mount RJ11 Extender Connector Kit

Product Line
CM3000
CM4000
PM800

Environment
Panel Mount Connector Kits

Cause
Determining extender connector kits for powerlogic devices

Resolution
The Panel Mount RJ11 Extender Connector Kit is used for circuit monitors and power meters that have no display. This Extender module can be installed to run a cable and an RJ11 port to the front panel of the gear that contains the monitor. That way a person with a handheld remote display can walk up to a panel and plug in the display using the external RJ11 port.

The part number for the RJ11 Extender Kit is RJ11EXT.

The attached document is the documentation for the 
Panel Mount RJ11 Extender Connector Kit
 
Was this helpful?
What can we do to improve the information ?