Technical FAQs

Ask a Question

Where to get a case for a Portable CM4000?

Product Line
PCM4

Resolution

Schneider Electric does not currently sell a case for the PCM4 portable circuit monitor. The recommendation is to buy a Tool case with wheels and a telescoping handle.

The minimum inside dimensions required to fit the meter + cables + Clamp-on CTs are:

23 inches by 15 inches by 11 inches.

The following links are to web sites that may offer appropriate cases.

Click the link: http://www.plattcases.com or http://www.justcases.com/delwheelship.html

Was this helpful?
What can we do to improve the information ?