Technical FAQs

Ask a Question

Can an IP address be written to a register when setting up a CM2000 or CM4000 with an ECC

Issue
Can an IP address be written to a CM2000 or CM4000 register?

Product Line
CM4000
CM2000
ECM2000
ECMRM

Environment
Register Mapping

Cause
Instead of using a front display can an IP address be written to a register

Resolution
Yes, both the CM2000 and the CM4000 can have an IP address written to a register. These registers are 6995 through 6999.
Was this helpful?
What can we do to improve the information ?