Technical FAQs

Ask a Question

What tools are required to install or remove CVM or CVMT?

Product Line
Current/Voltage Module (CVM)
Current/Voltage Module Transient (CVMT)
CM4000 Series Meters
CM3000 Series Meters

Environment
Hardware installation

Resolution


For any installation or removal of the CVM/CVMT remove control power from the meter.
The terminal cover is attached using PH1 screws. The CVM/CVMT is attached using 3mm Allen/Hex wrench fasteners. 

Attached below is the installation manual for the CVM and the CVMT

 
Was this helpful?
What can we do to improve the information ?