Technical FAQs

Ask a Question

Why do I get Error Message: "16 bit window subsystem - hidden console" "WOWVDM", error while in NXT environment setup.

This is one of a few error messages that is encountered when running a 16-bit Windows
application or an MS_DOS application in the NT environment.

The information including Symptoms, Cause, and Resolution on this error has been

published at the Microsoft Support Web Site :

http://support.microsoft.com/support/kb/articles/Q142/0/26.asp in Article ID : Q142026

Titled Err: "Hidden Console of WOW VDM" Running 16-BIT or MS-DOS App


Legacy KB System (APS) Data: RESL6007 V2.0, Originally authored by on , Last Edited by on
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?