Technical FAQs

Ask a Question

How do I assign variables when using multiple pens in a Magelis curve object application using XBTL1000 software ?

The variables are automatically assigned as contiguous registers based on the number of pens used.

Was this helpful?
What can we do to improve the information ?