Technical FAQs

Ask a Question

What would cause ProWORX NxT "Message (42) Path/File access error: ERR=00075, ERL=04765"?

Here are the two options to try and clear the Path File Access error:

1- The "Path File Access" error can occur when the ProWORX NxT file attributes have been changed over to "Read-only". Transferring them from a CD will cause this. Go into the ProWORX NxT file Properties and make sure the file attributes show "Archive". If "Read-only" is checked, uncheck and apply. This will clear the "Path File Access" error.
2- The "Path File Access" error usually has to do with Administrator rights on the PC. You should have full administrator rights on the PC and log on as Administrator. This will also clear the "Path File Access" error.


Legacy KB System (APS) Data: RESL5988 V3.0, Originally authored by RoAl on 03/29/2012, Last Edited by RoAl on 03/29/2012
Related ranges: ProWORX
Was this helpful?
What can we do to improve the information ?