Technical FAQs

Ask a Question

When using Concept 2.5 SR1 for IEC HSBY applications, is there a limit to the size of the project ?

Yes. Concept 2.5 SR1 will limit IEC HSBY applications to 1024 Kbytes.


Legacy KB System (APS) Data: RESL5928 V2.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?