Technical FAQs

Ask a Question

What is included in the 170XTS00900 Interbus S connector kit?

The 170XTS00900 Interbus S connector kit comes with two non low profile 9-pin connectors, one male and one female. Also included is an insertion tool, which is attached to the end of a standard flat screwdriver, allowing the wires to be inserted into the slots of the connectors.


Legacy KB System (APS) Data: RESL5884 V5.0, Originally authored by MiRo on 03/05/2008, Last Edited by DaSo on 08/20/2013
Related ranges: Interbus-S
Was this helpful?
What can we do to improve the information ?