Technical FAQs

Ask a Question

Does SQL Server 7.0 provided with Monitor Pro 7 have limitations?

No. The SQL Server provided with Monitor Pro is Microsofts standard SQL Server 7.0 software and there are no special limitations imposed, but it is intended for use with Monitor Pro and not as a standalone database product.


Legacy KB System (APS) Data: RESL5855 V2.0, Originally authored by on , Last Edited by on
Related ranges: MPRO CLIENT SERVER
Was this helpful?
What can we do to improve the information ?