Technical FAQs

Ask a Question

How many CALs (SQL Server Client) are included with the SQL Server 7 package that is bundled with Monitor Pro?

Each Monitor Pro 7 Server contains a SQL Server 7.0 license and each Monitor Pro 7 CAL (part number -MP CAL) includes a SQL Server CAL. There are no additional SQL Server CALs supplied with the software, but users may purchase additional SQL Server CALs from Microsoft if necessary.

Was this helpful?
What can we do to improve the information ?