Technical FAQs

Ask a Question

Can I Delete the Fast Task in PL7 Software?

No you can't, delete the fast task once you have created it.
A work around to accomplish this :
 

Step
Action
1
Export the application
2
Create a new application
3
Configure the new application modules and racks as in the old application
4
Import the exported application
5
Do not create a fast task

Or , you can leave the fast task and inhibit the task by resetting the %S31 bit to 0
(1 = activation of the fast task)

Legacy KB System (APS) Data: RESL5804 V2.0, Originally authored by on , Last Edited by on
Related ranges: PL7
Was this helpful?
What can we do to improve the information ?