Technical FAQs

Ask a Question

How many uni-telway addresses does the TSX 37Micro/TSX57Premium terminal port support?

The maximum number of uni-telway addresses supported by the terminal port in master mode is 8.
Addresses 1,2,3 are reserved for the programming device. therefore, only addresses 4,5,6,7,8 are available.

Was this helpful?
What can we do to improve the information ?