Technical FAQs

Ask a Question

Why do I get an " Invalid NetBios command Modbus Error code 803" when trying to connect MB+ using Modsoft?

The reason is the PLC address you entered does not exist on the network. Make sure the PLC address is valid.

Was this helpful?
What can we do to improve the information ?