Technical FAQs

Ask a Question

What is the minimum screen resolution to be used with Concept 2.6?

The minimum screen display resolution for Concept 2.6 is 800 x 600 pixels. This is a change from earlier versions which allowed 640 x 480 pixels.


Legacy KB System (APS) Data: RESL2555 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?