Technical FAQs

Ask a Question

WIll the MB + card work with a Texas Instruments 1420 Cardbus controller?

There is a known issue with the Texas Instrument 1420 Cardbus Controller. Schneider has determined the issue resides with the computer manufactures BIOS with relation to Windows 2000 & XP operating systems . Recently Schneider has been able to get some issues resolved by updating the system BIOS or PCMCIA.SYS files from the computer manufacture. A BIOS update will not guarantee to resolve all issues with our Modbus Plus adapters.


Legacy KB System (APS) Data: RESL2485 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modbus Plus
Was this helpful?
What can we do to improve the information ?