Technical FAQs

Ask a Question

Why are there no 4XXX registers configured for my analog input module ADU206 in Proworx with the TSX Compact E258/265/275/285 ?

When using the E258/265/275/285 the module's configuration data is found card config screen of Proworx..

Was this helpful?
What can we do to improve the information ?