Technical FAQs

Ask a Question

How can I determine the scan time of the models 100-700 SY/MAX PLCs?

Scan time (in milliseconds) is displayed on the ON-LINE PLC STATUS page in SY/MATE software for the models 100-700 SY/MAX controllers. It is also displayed in register 8172.


Legacy KB System (APS) Data: RESL2438 V1.0, Originally authored by on , Last Edited by on
Related ranges: Sy/Max
Was this helpful?
What can we do to improve the information ?