Technical FAQs

Ask a Question

Why can't I see my M1E IP configuration when doing a scan bus with Concept Ethernet configuration tool?

The M1E controllers will not be seen, only Momentum slave bases with Ethernet communication adapters (ENTs). The Ethernet configuration tool was designed to work with the Ethernet communication adapters and not meant for the M1E's.


Legacy KB System (APS) Data: RESL2426 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?