Technical FAQs

Ask a Question

Why must I supply power to the AS-BADU-211 analog input module prior to powering the CPU?

If left unpowered, the AS-BADU-211 will try to pull power from the 5 volt supply on the CPU. As a result of this the BADU-211 will give a false ready and active indication. Although the module is providing correct indications the analog input signals will not be read correctly. Always power up this module prior to the CPU.

Was this helpful?
What can we do to improve the information ?