Technical FAQs

Ask a Question

Will my 140 EHC 202 00 maintain count values after a power failure?

No. The count values are not retentative. When the 140 EHC 202 00 experiences a power failure it will reset the counter registers. You may want to store the counter value in a different register so that it can be retrieved /restored in the event of a power failure or planned outage. T.


Legacy KB System (APS) Data: RESL2387 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?