Technical FAQs

Ask a Question

Is Profibus supported in a Quantum Hot Standby System?

No. The only Fieldbus that is supported for the control of I/O in a Quantum system is S908 Remote I/O. The Profibus module does not look at the status of the controllers with any regard for Primary or Standby and will result in both the Primary and the standby trying to control the I/O.


Legacy KB System (APS) Data: RESL2376 V1.0, Originally authored by on , Last Edited by on
Related ranges: Profibus DP
Was this helpful?
What can we do to improve the information ?