Technical FAQs

Ask a Question

Is it possible to program the TSX Premium via the ETY module ?

Yes, it is possible to establish a programming connection via TCP IP to the ETY modules or the Integrated PORT on some processors.
Programming via TCP IP requires the installation and configuration of the XIP Driver.
Programming via Ethway is also possible for the ETY110 only.
These Drivers are supplied on the XWAY Driver CD - TLXCDDRV13M
Note:
The ETY Module must be configured with a TCP/IP and Xway address prior to being able to establishing a programming connection with the XIP Driver.
The initial configuration should be performed via the Unitelway driver connected to the processor TER port.


Legacy KB System (APS) Data: RESL2363 V2.0, Originally authored by on , Last Edited by on
Related ranges: CANopen
Was this helpful?
What can we do to improve the information ?