Technical FAQs

Ask a Question

What form of isolation do the Quantum analog modules use?

With few exceptions Quantum analog modules use solid state isolation. The exceptions would be the AII330 00, AII330 10 and AIO 330 00. These modules are Intrinsically Safe and offer galvanic isolation by way of an approved barrier which is shipped with the modules.


Legacy KB System (APS) Data: RESL2313 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?