Technical FAQs

Ask a Question

What are the different part#s for the Modicon 884 PLC?

The different part#'s for the Modicon 884 PLC are:
* AS-884A-101 - 2K with 1 Modbus port
* AS-884A-111 - 2K with 2 Modbus ports
* AS-884A-201 - 3.5K with 1 Modbus port
* AS-884A-211 - 3.5 K with 2 Modbus ports
* AS-884A-301 - 8K with 1 Modbus port
* AS-884A-311 - 8K with 2 Modbus ports

 
Was this helpful?
What can we do to improve the information ?