Technical FAQs

Ask a Question

What is the part number for the terminal strip Isothermal bar that's used with the B883-200 Thermocouple Input Module?

The part number is AS-8643-000. The Isolated Thermo high density connector/cable duct assembly (AS-8643-000) is included with the B883-200 module. The terminal strip Isothermal Bar is used to perform CJC or RCJC temperature sensing. This is the only acceptable field connector for use with the B883-200


Legacy KB System (APS) Data: RESL2174 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon 1/2/3/4/5/8/984s
Was this helpful?
What can we do to improve the information ?