Technical FAQs

Ask a Question

What causes error 32600 in a SY/MAX controller?

Error code 32600 is the Hardware Diagnostic Error.
Possible causes:
1) May be any module in CPU rack (usually LI or LTI)
2) Module series incompatibility

Recovery procedure:
1) Check for series incompatibility. Determine if a Model 700 processor is used with pre-series C Analog or pre-series H Local Interface module in CPU rack. Both modules will not operate properly in CPU rack. Replace with later series modules.
2) Switch power off. Check power supply according to Section 2 of Troubleshooting Guide.
3) Replace LI, CPU or any modules in the rack where needed.

Was this helpful?
What can we do to improve the information ?