Technical FAQs

Ask a Question

If the power is removed from the Twido PLC, will the Real Time Clock part number TWDXCPRTC, continue to be updated?

Yes. Using a fully charged battery the time will continue to be updated for 1000 hours at 25 degrees C or 300 hours at 55 degrees C .


Legacy KB System (APS) Data: RESL2162 V1.0, Originally authored by on , Last Edited by on
Related ranges: Twido
Was this helpful?
What can we do to improve the information ?