Technical FAQs

Ask a Question

What are the storage temperature ratings for the M340 PLC ?

The non-operational climate specifications are documented in the Modicon M340 Processors, Racks, and Power Supply Modules User Guide as shown below:


Legacy KB System (APS) Data: RESL213097 V1.0, Originally authored by DaSo on 12/06/2013, Last Edited by DaSo on 12/06/2013
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?