Technical FAQs

Ask a Question

How many wires can you put on a terminal on an Advantys I/O module?

Wiring specifications for the Advantys I/O is that you can only put one wire in a terminal and it can be between 18 and 24 gage.

Legacy KB System (APS) Data: RESL213080 V1.0, Originally authored by DiSa on 12/05/2013, Last Edited by DiSa on 12/05/2013
Related ranges: Modicon STB
Was this helpful?
What can we do to improve the information ?