Technical FAQs

Ask a Question

Does Schneider Electric sell the optional electrolytic caps for the Quantum power supplies?

No. The manual references optional capacitors that you could use depending on the input voltage and hold-up time. This is just reference information and depending on what your requirement is, the chart will tell you the size of capacitor you should purchase in mF, (micro-farad). These parts can be purchased form a local electronics store like a Radio Shack.


Was this helpful?
What can we do to improve the information ?