Technical FAQs

Ask a Question

What does FUN 41 mean on a Model 50 Hand Held Programmer?

FUN 41 is a function code for the hand held programmer.
FUN41 is shutdown / auto-restart mode selection.

If set to 0, it will be in shutdown mode
If set to 1, it will be in auto-restart mode.

Was this helpful?
What can we do to improve the information ?