Technical FAQs

Ask a Question

What is the meaning of a LdoG - Unknown system error in a Lexium32 drive?

This error is an internal system error, LdoG = wdog ( watchdog). The internal communication of the controller board is supervised and the drive reports a problem.
If you get this error, power down your Lexium32 drive, remove all modules (applies only to Lexium32M) and the memory card if there is one. Power up your Lexium32 drive. If the error still occurs, you must replace the drive.

Was this helpful?
What can we do to improve the information ?