Technical FAQs

Ask a Question

Does the M340 product line meet the "Finger Safe" or IEC 60529 specification?

IEC 60529 is the standard for Ingress Protection. The M340 product line is IP20 rated which is considered "Finger Safe"

 
 
 
text
 
 
text

Legacy KB System (APS) Data: RESL213047 V1.0, Originally authored by DaSo on 12/05/2013, Last Edited by DaSo on 12/05/2013
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?